San - Antimicrobial
Flat retaining magnets
Flat retaining magnets
A rich selection of flat magnets that provides solutions to permanent fixing problems in different application areas. Available in the range: flat magnets with containment body in galvanized steel lacquered in red, stainless steel and disk in galvanized steel, or with anti-slip coating in thermoplastic elastomer.
Different construction materials (ferrite magnets, aluminum, nickel, cobalt magnets, samarium cobalt magnets, and neodymium iron boron) offer specific values of attraction strength, resistance to temperatures, corrosion, workability, and the possibility of demagnetization. Because of their structure, these industrial magnets only have one attraction surface that concentrates all the magnetic energy. The effect in space of the magnetic field is limited by a shielding system, which results in the surrounding objects not being magnetized.