HCV-E-LD Electrical level indicators with LED

with MIN level electrical sensor, transparent technopolymer

 
 

Select item

loading

Technical specifications

Scroll horizontally
Main specifications

Material

Transparent polyamide based (PA-T) technopolymer. Highly resistant to shocks, solvents, oils with additives, aliphatic and aromatic hydrocarbons, petrol, naphtha, phosphoric esters.

Avoid contact with alcohol or detergents containing alcohol.

Screws, nuts and washers

Zinc-plated steel.

Packing rings

Step-shaped for the seal on the reservoir walls and NBR synthetic rubber O-ring screw underhead.

Suggested roughness of the packing ring application surface Ra = 3 µm.

Float

Glass-fibre reinforced polyamide based (PA) technopolymer, black colour, with a built-in magnetic element to activate the electric contact when the float reaches the contact threshold indicated in the drawing (data referred to mineral oil type CB68, according to ISO 3498, temperature 23°C).

Floating is ensured by fluids with densities higher than 800 kg/m3.

Bracket with male connector

Perfectly watertight, incorporating the reed with three conductors (SW) and the LED. 8-pin M12x1 connector with threading in glass-fibre reinforced polyamide based (PA) technopolymer certified self-extinguishing UL-94-V0, black colour, matte finish.

For a correct assembly see Warnings.

Contrast screen

White lacquered aluminium. The housing, in the appropriate external rear slot, guarantees the best protection from direct contact with fluid.

It can be taken out from the inclined side, before assembly to allow the insertion of level lines or words.

Standard executions

  • HCV-E-NO-LD: the electrical contact closes on reaching the minimum level and the LED changes from green to red.
  • HCV-E-SW-LD: the electrical change-over contact switches between the two clamps when the minimum level is reached and the LED changes from green to red.

Maximum continuous working temperature

90°C (with oil).

General information

Features and performances

The HCV-E-LD level indicators, in addition to the visual level indicator, also provide an electrical signal when the minimum fluid level value is reached and a green or red light signal indicating the presence or absence of fluid respectively.

The switching of the electrical signal is simultaneous with the switching of the indicator light.

The lateral connector output allows the level of intervention of the sensor to be minimised.

Ultrasound welding to guarantee a perfect seal.

Maximum fluid level visibility even from side positions.

Lens effect for a better visibility of the fluid level.

In case of use of an extension, the direction of the cable output is shown in Fig.1..

Technical data

In laboratory tests carried out with mineral oil type CB68 (according to ISO 3498) at 23°C for a limited period of time, the weld stood up to: 18 bar (HCV.76), 18 bar (HCV.127) and 12 bar (HCV.254).

For use with fluids other than mineral oils and under particular different pressure and temperature conditions, please contact ELESA Technical Department.

In any case we suggest to verify the suitability of the product under the actual working conditions.

HCV-E-NO-LD - with normally open contact 
Electrical features
Electrical featuresMIN level sensor
Power supplyAC/DC
Electric contactsNO normally open
SW change-over contact
Maximum applicable voltageNO: 48 Vdc
SW: 48 Vdc
Maximum switching current1 A (Input Vsf)
0.3A at 25°C (input Vin)
Maximum currentNO: 1.2A
SW: 2A
Maximum commutable powerNO: 10 Va
SW: 20 Va
ConnectorM12x1
Do not mount this indicator in proximity to magnetic fields.
HCV-E-NO-LD - with normally open contact 
Instructions of use

Wiring instructions

Connect the positive power supply to the Vin or Vsf pin. The Vin pin has overcurrent protection which is limited to 300mA (at 25°C).

The current at the Vsf pin input must be limited with a fuse or equivalent protection provided by the user so as not to exceed the maximum values ​​indicated in the electrical features table.

Connect the negative power supply to pins 3, 4, 5, and 8.

When the device is not activated, i.e. the liquid level is not below the minimum level and the LED is green, the positive power supply applied to the Vin or Vsf pin will be present on the NC contact (pin 1) – only in the case of a device with a change-over contact (SW).

When the device is activated, i.e. the liquid level is below the minimum level and the LED is red, the positive power supply applied to the Vin or Vsf pin will be present on the NO contact (pin 2).

Other executions

Special executions on request

  • Level indicators with stainless steel screws, nuts and washers.
  • Level indicators HCV.76 with screws M12.
  • Level indicators for use with fluids containing alcohol.
  • UV resistant transparent technopolymer level indicators.
Accessories on request

Accessories on request

FC-M12x1: extensions with 8 pole M12 female axial connector.

Elesa
Models all rights reserved in accordance with the law. Always mention the source when reproducing our drawings and photos.

ASK THE EXPERT