SELF-SANITISATION AGAINST BACTERIA AND FUNGI
No-slip disks for levelling elements
It is extremely important that the no-slip disk must not detach from the base of the levelling element.
There are typical situations in which the conditions for the detachment of the no-slip disk could take place:
- case of eventual “sticking” of the no-slip disk to the floor while lifting the machinery for moving;
- case of side impacts against the levelling element with the no-slip disk during machinery transport.
The assembling system created by Elesa consists of an anchoring in the central part of the disk, besides a particular slot along the whole rim profile.
Tests of separation, carried out in our labs with suitable equipment simulating real conditions (Fig. 1 and Fig. 2), have given the following results, compared with the current anchoring systems:
- detachment resistance in cases of adhesion (sticking) of the noslip disk to the floor: fourfold increased;
- detachment resistance in case of side impacts: tenfold increased.
The no-slip disks are supplied assembled to their plastic bases.


-
GENERAL
-
ADJUSTABLE LEVERS
-
HANDLE WITH PNEUMATIC DRIVE
-
GRADUATIONS
-
ROTARY CONTROLS
-
BALL TRANSFER UNITS
-
MODULAR ROLLER TRACKS
-
LEVEL BUBBLES
-
SPUR GEARS
-
RUBBER BUFFERS
-
HIGH PERFORMANCE VIBRATION DAMPERS
-
MAGNETS
-
LEVELLING FEET
-
HYGIENIC DESIGN
-
HINGES
-
PNEUMATIC FASTENING CLAMPS
-
ELECTRICAL LEVEL INDICATORS
-
CASTORS AND WHEELS
-
Vacuum components
-
Elastomer springs