San - Antimicrobial
Elesa - Wheels that combine smoothness and maneuverability
Nov 12, 2018
Reading time: minutes
The “soft” polyurethane is particularly resistant to wear, a feature that makes the RE.F2 series wheels ideal for use in environments with the presence of atmospheric agents, alcohols and glycols. Thanks to these qualities, the wheels represent an ideal solution for both outdoor and indoor applications. The soft cast polyurethane gives the Elesa RE.F2 wheels great elasticity, improving their smoothness, to the advantage of maneuverability even with heavy loads. The elasticity also allows greater absorption of shocks and vibrations. The resistance to wear and tear allows less force to be used to push or pull the trolleys. The RE.F2 wheels are also supplied with different types of steel supports, depending on the application.